ChannelFittingBuilder Class¶
-
class
NXOpen.Tooling.
ChannelFittingBuilder
¶ Bases:
NXOpen.Builder
The builder class for Channel Fitting which assists you to add cooling fitting.
To create a new instance of this class, use
NXOpen.Tooling.ChannelFittingCollection.CreateChannelFittingBuilder()
Default values.
Property Value BottomClearance.Value 0 (millimeters part), 0 (inches part) TopClearance.Value 5 (millimeters part), 1.25 (inches part) UseSymbol 1 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
BottomClearance | Returns the bottom clearance |
BoundaryBody | Returns the boundary body to create the cooling fitting points. |
FittingPoint | Returns or sets the new point specified for the cooling fitting point. |
ParentChannel | Returns the parent channel of the cooling fitting points. |
SearchBoundaryBodies | Returns or sets the value which specifies whether to auto search boundary bodies or not. |
Tag | Returns the Tag for this object. |
TopClearance | Returns the top clearance |
UseSymbol | Returns or sets the value which specifies whether to add real component or not. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateCoolingFittingData | Creates the Cooling Fitting Data object. |
CreateFittingPoints | Create Fitting Points. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCoolingFittingData | Get the Cooling Fitting Data object. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BottomClearance¶
-
ChannelFittingBuilder.
BottomClearance
¶ Returns the bottom clearance
-------------------------------------
Getter Method
Signature
BottomClearance()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
BoundaryBody¶
-
ChannelFittingBuilder.
BoundaryBody
¶ Returns the boundary body to create the cooling fitting points.
-------------------------------------
Getter Method
Signature
BoundaryBody()
Returns: Return type: NXOpen.SelectBodyList
New in version NX8.0.0.
License requirements: None.
FittingPoint¶
-
ChannelFittingBuilder.
FittingPoint
¶ Returns or sets the new point specified for the cooling fitting point.
-------------------------------------
Getter Method
Signature
FittingPoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FittingPoint(fittingPoint)
Parameters: fittingPoint ( NXOpen.Point
) –New in version NX7.5.0.
License requirements: None.
ParentChannel¶
-
ChannelFittingBuilder.
ParentChannel
¶ Returns the parent channel of the cooling fitting points.
-------------------------------------
Getter Method
Signature
ParentChannel()
Returns: Return type: NXOpen.SelectBodyList
New in version NX7.5.0.
License requirements: None.
SearchBoundaryBodies¶
-
ChannelFittingBuilder.
SearchBoundaryBodies
¶ Returns or sets the value which specifies whether to auto search boundary bodies or not.
-------------------------------------
Getter Method
Signature
SearchBoundaryBodies()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SearchBoundaryBodies(searchBoundaryBodies)
Parameters: searchBoundaryBodies (bool) – New in version NX8.0.0.
License requirements: None.
TopClearance¶
-
ChannelFittingBuilder.
TopClearance
¶ Returns the top clearance
-------------------------------------
Getter Method
Signature
TopClearance()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
UseSymbol¶
-
ChannelFittingBuilder.
UseSymbol
¶ Returns or sets the value which specifies whether to add real component or not.
-------------------------------------
Getter Method
Signature
UseSymbol()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseSymbol(useSymbol)
Parameters: useSymbol (bool) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”)
Method Detail¶
CreateCoolingFittingData¶
-
ChannelFittingBuilder.
CreateCoolingFittingData
¶ Creates the Cooling Fitting Data object.
Signature
CreateCoolingFittingData()
Returns: the new Tooling.CoolingFittingData
instanceReturn type: NXOpen.Tooling.CoolingFittingData
New in version NX7.5.0.
License requirements: None.
CreateFittingPoints¶
-
ChannelFittingBuilder.
CreateFittingPoints
¶ Create Fitting Points.
Signature
CreateFittingPoints()
New in version NX7.5.0.
License requirements: None.
GetCoolingFittingData¶
-
ChannelFittingBuilder.
GetCoolingFittingData
¶ Get the Cooling Fitting Data object.
Signature
GetCoolingFittingData()
Returns: Return type: NXOpen.Tooling.CoolingFittingData
New in version NX7.5.0.
License requirements: None.
Validate¶
-
ChannelFittingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.