ChannelAdjustBuilderVectorMethod Enumeration

NXOpen.Tooling.ChannelAdjustBuilder.VectorMethod is an alias for NXOpen.Tooling.ChannelAdjustBuilderVectorMethod

class NXOpen.Tooling.ChannelAdjustBuilderVectorMethod

Bases: object

the vector adjust method.

Enum Members

Enum Member Enum Member Description
Along
Reposition the target channels along the vector specified.
Perpendicular
Reposition the target channels Perpendicular the vector specified.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.