ChannelAdjustBuilderAdjustType Enumeration

NXOpen.Tooling.ChannelAdjustBuilder.AdjustType is an alias for NXOpen.Tooling.ChannelAdjustBuilderAdjustType

class NXOpen.Tooling.ChannelAdjustBuilderAdjustType

Bases: object

the adjust method.

Enum Members

Enum Member Enum Member Description
Distance
Reposition the target channels.
BaffleLength
Change the length of the baffles.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.