ChangeoverManagementBuilderTypes Enumeration

NXOpen.Tooling.ChangeoverManagementBuilder.Types is an alias for NXOpen.Tooling.ChangeoverManagementBuilderTypes

class NXOpen.Tooling.ChangeoverManagementBuilderTypes

Bases: object

Specifies the types of changeover management.

Enum Members

Enum Member Enum Member Description
Create
the create mode
Manage
the manage mode
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.