CaeReuseLibrary Class¶
-
class
NXOpen.Tooling.
CaeReuseLibrary
¶ Bases:
object
Represents a
NXOpen.Tooling.CaeReuseLibrary
To obtain an instance of this class, refer to
NXOpen.CAE.BaseFEModel
New in version NX7.5.2.
Methods¶
Method | Description |
---|---|
CreateReusableObject | Creates a NXOpen.Tooling.ReusableObject @return NXOpen.Tooling.ReusableObject |
ExportBeamSectionToLibrary | Exports a beam section to created reuse library |
ImportBeamSectionFromLibrary | Copies a beam section from library to current part @return Beam section created by the given library |
UpdateDescription | Renames and updates preview image for reusable object |
Method Detail¶
CreateReusableObject¶
-
CaeReuseLibrary.
CreateReusableObject
¶ Creates a
NXOpen.Tooling.ReusableObject
Signature
CreateReusableObject()
Returns: NXOpen.Tooling.ReusableObject
Return type: NXOpen.Tooling.ReusableObject
New in version NX7.5.2.
License requirements: None.
ExportBeamSectionToLibrary¶
-
CaeReuseLibrary.
ExportBeamSectionToLibrary
¶ Exports a beam section to created reuse library
Signature
ExportBeamSectionToLibrary(reuseLibraryName, reusableObject)
Parameters: - reuseLibraryName (str) – Library to which beam-section is exported
- reusableObject (
NXOpen.Tooling.ReusableObject
) –NXOpen.Tooling.ReusableObject
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ImportBeamSectionFromLibrary¶
-
CaeReuseLibrary.
ImportBeamSectionFromLibrary
¶ Copies a beam section from library to current part
Signature
ImportBeamSectionFromLibrary(reuseLibraryName)
Parameters: reuseLibraryName (str) – Library from where beam-section is imported Returns: Beam section created by the given library Return type: NXOpen.CAE.BeamSection
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
UpdateDescription¶
-
CaeReuseLibrary.
UpdateDescription
¶ Renames and updates preview image for reusable object
Signature
UpdateDescription(descriptiveName, reuseLibraryName, previewImageFile)
Parameters: - descriptiveName (str) – New descriptive name
- reuseLibraryName (str) – Library to update
- previewImageFile (str) – New preview image file name including the path
New in version NX7.5.2.
License requirements: None.