BurringInsertBuilderBurringPunchTypes Enumeration

NXOpen.Tooling.BurringInsertBuilder.BurringPunchTypes is an alias for NXOpen.Tooling.BurringInsertBuilderBurringPunchTypes

class NXOpen.Tooling.BurringInsertBuilderBurringPunchTypes

Bases: object

Specifies the burring punch type.

Enum Members

Enum Member Enum Member Description
First
use first type
Second
use second type
Third
use third type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.