BurringInsertBuilderBurringDirections Enumeration

NXOpen.Tooling.BurringInsertBuilder.BurringDirections is an alias for NXOpen.Tooling.BurringInsertBuilderBurringDirections

class NXOpen.Tooling.BurringInsertBuilderBurringDirections

Bases: object

Specifies the burring direction.

Enum Members

Enum Member Enum Member Description
BurringUpwards
design the burring upwards
BurringDownwards
design the burring downwards
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.