BomBuilderTreeList Enumeration

NXOpen.Tooling.BomBuilder.TreeList is an alias for NXOpen.Tooling.BomBuilderTreeList

class NXOpen.Tooling.BomBuilderTreeList

Bases: object

Represents an index to components list type.

Enum Members

Enum Member Enum Member Description
Bom
A list includes components in BOM
Hide
A list includes hidden components
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.