BomBuilderShape Enumeration

NXOpen.Tooling.BomBuilder.Shape is an alias for NXOpen.Tooling.BomBuilderShape

class NXOpen.Tooling.BomBuilderShape

Bases: object

Represents an index to the shape of stock size.

Enum Members

Enum Member Enum Member Description
Rectangular
The rectangular type.
Circular
The circular type.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.