BomBuilderCircle Enumeration

NXOpen.Tooling.BomBuilder.Circle is an alias for NXOpen.Tooling.BomBuilderCircle

class NXOpen.Tooling.BomBuilderCircle

Bases: object

Represents an index to the base circle type of cylinder shape.

Enum Members

Enum Member Enum Member Description
Circumcircle
Circumcircle.
InscribedCircle
Inscribed circle.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.