BlankNestingBuilder Class¶
-
class
NXOpen.Tooling.
BlankNestingBuilder
¶ Bases:
NXOpen.Builder
Blank Nesting Builder of PDW, EDW and Die Engineering.
No object is returned by this builder. To create a new instance of this class, use
NXOpen.Tooling.BlankNestingCollection.CreateBlankNestingBuilder()
Default values.
Property Value AngleResult 0 AngleStep 25 BlankArea 0 BoundarySegment 200 HeightStep 25 LayoutType Rectangle MinimumDistance 0 PitchResult 0 StripWidthResult 0 Utilization 0 WebDistance 0 New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
AngleResult | Returns or sets the angle between processed blank and original blank. |
AngleStep | Returns or sets the angle increment to use when rotating the blank during the processing to find the best layout. |
BlankArea | Returns or sets the up datum face area that was found in the processing. |
BoundarySegment | Returns or sets the number of boundary segment. |
HeightStep | Returns or sets the distance increment to use when translating the blank in the vertical direction during the processing to find the best layout. |
LayoutType | Returns or sets the type of layout to use in the blank nesting processing. |
MinimumDistance | Returns or sets the minimum distance between the adjacent blanks. |
PitchResult | Returns or sets the distance between blanks that was found in the processing. |
SelectObject | Returns the selected entities making up the blank to be nested. |
StripWidthResult | Returns or sets the strip width. |
Tag | Returns the Tag for this object. |
Utilization | Returns or sets the maximum material utilization of the blank. |
WebDistance | Returns or sets the distance between the blank and the strip. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
LayoutCalculation | The method to calculate maximum material utilization for the selected entities. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BlankNestingBuilderLayoutTypeSpecification Enumeration | Specifies the layout type of blank nesting. |
Property Detail¶
AngleResult¶
-
BlankNestingBuilder.
AngleResult
¶ Returns or sets the angle between processed blank and original blank.
-------------------------------------
Getter Method
Signature
AngleResult()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleResult(angleResult)
Parameters: angleResult (float) – New in version NX8.5.0.
License requirements: None.
AngleStep¶
-
BlankNestingBuilder.
AngleStep
¶ Returns or sets the angle increment to use when rotating the blank during the processing to find the best layout.
The angle is specified in degrees.
-------------------------------------
Getter Method
Signature
AngleStep()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleStep(angleStep)
Parameters: angleStep (float) – New in version NX8.5.0.
License requirements: None.
BlankArea¶
-
BlankNestingBuilder.
BlankArea
¶ Returns or sets the up datum face area that was found in the processing.
-------------------------------------
Getter Method
Signature
BlankArea()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlankArea(blankArea)
Parameters: blankArea (float) – New in version NX8.5.0.
License requirements: None.
BoundarySegment¶
-
BlankNestingBuilder.
BoundarySegment
¶ Returns or sets the number of boundary segment.
-------------------------------------
Getter Method
Signature
BoundarySegment()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundarySegment(boundarySegment)
Parameters: boundarySegment (int) – New in version NX8.5.0.
License requirements: None.
HeightStep¶
-
BlankNestingBuilder.
HeightStep
¶ Returns or sets the distance increment to use when translating the blank in the vertical direction during the processing to find the best layout.
-------------------------------------
Getter Method
Signature
HeightStep()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HeightStep(heightStep)
Parameters: heightStep (float) – New in version NX8.5.0.
License requirements: None.
LayoutType¶
-
BlankNestingBuilder.
LayoutType
¶ Returns or sets the type of layout to use in the blank nesting processing.
-------------------------------------
Getter Method
Signature
LayoutType()
Returns: Return type: NXOpen.Tooling.BlankNestingBuilderLayoutTypeSpecification
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LayoutType(layoutType)
Parameters: layoutType ( NXOpen.Tooling.BlankNestingBuilderLayoutTypeSpecification
) –New in version NX8.5.0.
License requirements: None.
MinimumDistance¶
-
BlankNestingBuilder.
MinimumDistance
¶ Returns or sets the minimum distance between the adjacent blanks.
-------------------------------------
Getter Method
Signature
MinimumDistance()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimumDistance(minimumDistance)
Parameters: minimumDistance (float) – New in version NX8.5.0.
License requirements: None.
PitchResult¶
-
BlankNestingBuilder.
PitchResult
¶ Returns or sets the distance between blanks that was found in the processing.
-------------------------------------
Getter Method
Signature
PitchResult()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PitchResult(pitchResult)
Parameters: pitchResult (float) – New in version NX8.5.0.
License requirements: None.
SelectObject¶
-
BlankNestingBuilder.
SelectObject
¶ Returns the selected entities making up the blank to be nested.
-------------------------------------
Getter Method
Signature
SelectObject()
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
StripWidthResult¶
-
BlankNestingBuilder.
StripWidthResult
¶ Returns or sets the strip width.
-------------------------------------
Getter Method
Signature
StripWidthResult()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StripWidthResult(stripWidthResult)
Parameters: stripWidthResult (float) – New in version NX8.5.0.
License requirements: None.
Utilization¶
-
BlankNestingBuilder.
Utilization
¶ Returns or sets the maximum material utilization of the blank.
-------------------------------------
Getter Method
Signature
Utilization()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Utilization(utilization)
Parameters: utilization (float) – New in version NX8.5.0.
License requirements: None.
WebDistance¶
-
BlankNestingBuilder.
WebDistance
¶ Returns or sets the distance between the blank and the strip.
-------------------------------------
Getter Method
Signature
WebDistance()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WebDistance(webDistance)
Parameters: webDistance (float) – New in version NX8.5.0.
License requirements: None.
Method Detail¶
LayoutCalculation¶
-
BlankNestingBuilder.
LayoutCalculation
¶ The method to calculate maximum material utilization for the selected entities.
Signature
LayoutCalculation()
New in version NX8.5.0.
License requirements: None.
Validate¶
-
BlankNestingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.