BlankLayoutBuilderTypes Enumeration

NXOpen.Tooling.BlankLayoutBuilder.Types is an alias for NXOpen.Tooling.BlankLayoutBuilderTypes

class NXOpen.Tooling.BlankLayoutBuilderTypes

Bases: object

Specifies the option of blank layout type.

Enum Members

Enum Member Enum Member Description
CreateLayout
the type of create blank layout
AddBlank
the type of add multiple blank
CopyBlank
the type of copy blank
RemoveBlank
the type of remove blank
SetBasePoint
the type of set the base point of the blank
FlipBlank
the type of flip blank
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.