BlankLayoutBuilderSnapSizeOption Enumeration¶
NXOpen.Tooling.BlankLayoutBuilder.SnapSizeOption is an alias for NXOpen.Tooling.BlankLayoutBuilderSnapSizeOption
-
class
NXOpen.Tooling.
BlankLayoutBuilderSnapSizeOption
¶ Bases:
object
Specifies the option of snap size.
Enum Members
Enum Member Enum Member Description Tenth the snap size is 0.1Fifth the snap size is 0.2Half the snap size is 1/2One the snap size is 1Two the snap size is 2Five the snap size is 5Ten the snap size is 10-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-