BlankLayoutBuilderSideWebOption Enumeration

NXOpen.Tooling.BlankLayoutBuilder.SideWebOption is an alias for NXOpen.Tooling.BlankLayoutBuilderSideWebOption

class NXOpen.Tooling.BlankLayoutBuilderSideWebOption

Bases: object

Specifies the option of side webs type.

Enum Members

Enum Member Enum Member Description
Average
the side webs type of average
Bottom
the side webs type of bottom
Top
the side webs type of top
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.