BendOperationCollection Class

class NXOpen.Tooling.BendOperationCollection

Bases: object

Creates a NXOpen.Tooling.BendOperationBuilder

To obtain an instance of this class, refer to NXOpen.Tooling.ToolingManager

New in version NX8.5.0.

Methods

Method Description
CreateBendOperationBuilder Creates a NXOpen.Tooling.BendOperationBuilder @return
FindObject Finds the NXOpen.Tooling.BendOperationBuilder with the given identifier as recorded in a journal.

Method Detail

CreateBendOperationBuilder

BendOperationCollection.CreateBendOperationBuilder

Creates a NXOpen.Tooling.BendOperationBuilder

Signature CreateBendOperationBuilder()

Returns:
Return type:NXOpen.Tooling.BendOperationBuilder

New in version NX8.5.0.

License requirements: None.

FindObject

BendOperationCollection.FindObject

Finds the NXOpen.Tooling.BendOperationBuilder with the given identifier as recorded in a journal.

An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.

An exception will be thrown if no object can be found with the given journal identifier.

Signature FindObject(journalIdentifier)

Parameters:journalIdentifier (str) – Identifier to be found
Returns:BendOperationBuilder found
Return type:NXOpen.Tooling.BendOperationBuilder

New in version NX8.5.0.

License requirements: None.