BendOperationBuilderTypes Enumeration

NXOpen.Tooling.BendOperationBuilder.Types is an alias for NXOpen.Tooling.BendOperationBuilderTypes

class NXOpen.Tooling.BendOperationBuilderTypes

Bases: object

unbend operations.

Enum Members

Enum Member Enum Member Description
Unbend
unbend operation
Rebend
rebend operation
Prebend
prebend operation
Overbend
overbend operation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.