BendInsertDesignBuilderBendingDirectionOption Enumeration

NXOpen.Tooling.BendInsertDesignBuilder.BendingDirectionOption is an alias for NXOpen.Tooling.BendInsertDesignBuilderBendingDirectionOption

class NXOpen.Tooling.BendInsertDesignBuilderBendingDirectionOption

Bases: object

the bending direction.

Enum Members

Enum Member Enum Member Description
Up
bending up
Down
bending down
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.