BendInsertDesignBuilderBendTypeOption Enumeration

NXOpen.Tooling.BendInsertDesignBuilder.BendTypeOption is an alias for NXOpen.Tooling.BendInsertDesignBuilderBendTypeOption

class NXOpen.Tooling.BendInsertDesignBuilderBendTypeOption

Bases: object

the bend type.

Enum Members

Enum Member Enum Member Description
Sbend
90 degree bend
Abend
angle bend
Zbend
z bend
Vbend
v bend
Uzbend
universal z bend
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.