AddReusablePartPositionMethod Enumeration

NXOpen.Tooling.AddReusablePart.PositionMethod is an alias for NXOpen.Tooling.AddReusablePartPositionMethod

class NXOpen.Tooling.AddReusablePartPositionMethod

Bases: object

Represents the position method

Enum Members

Enum Member Enum Member Description
Invalid
Absolute
Mate
Reposition
Wcs
Position
Point
Position by point
InferredOny
Routing
Position using Routing
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.