AddReusablePartPocketBodyMethod Enumeration¶
NXOpen.Tooling.AddReusablePart.PocketBodyMethod is an alias for NXOpen.Tooling.AddReusablePartPocketBodyMethod
-
class
NXOpen.Tooling.
AddReusablePartPocketBodyMethod
¶ Bases:
object
Represents save pocket body information, updating or deleting a pocket body size mode method
Enum Members
Enum Member Enum Member Description NotSet Save pocket body information into attatched componentUpdate Update the existed pocket body sizeDelete Delete pocket body-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-