AddReusablePartModeMethod Enumeration

NXOpen.Tooling.AddReusablePart.ModeMethod is an alias for NXOpen.Tooling.AddReusablePartModeMethod

class NXOpen.Tooling.AddReusablePartModeMethod

Bases: object

Represents adding or editing a reusable component mode method

Enum Members

Enum Member Enum Member Description
Add
Add reusable component
Edit
Edit reusable component
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.