ShapeSearchBuilderShapeSize Enumeration

NXOpen.ShapeSearch.ShapeSearchBuilder.ShapeSize is an alias for NXOpen.ShapeSearch.ShapeSearchBuilderShapeSize

class NXOpen.ShapeSearch.ShapeSearchBuilderShapeSize

Bases: object

The search shape size enum

Enum Members

Enum Member Enum Member Description
P90P110
search with shape size 90%-110% condition
P80P120
search with shape size 80%-120% condition
P70P130
search with shape size 70%-130% condition
P50P200
search with shape size 50%-200% condition
P25P400
search with shape size 25%-400% condition
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.