ShapeSearchBuilderShapeSimilarity Enumeration

NXOpen.ShapeSearch.ShapeSearchBuilder.ShapeSimilarity is an alias for NXOpen.ShapeSearch.ShapeSearchBuilderShapeSimilarity

class NXOpen.ShapeSearch.ShapeSearchBuilderShapeSimilarity

Bases: object

The search shape similarity enum

Enum Members

Enum Member Enum Member Description
Identical
search with identical condition
VerySimilar
search with very similar condition
Similar
search with similar condition
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.