ShapeSearchBuilderOpenPartType Enumeration

NXOpen.ShapeSearch.ShapeSearchBuilder.OpenPartType is an alias for NXOpen.ShapeSearch.ShapeSearchBuilderOpenPartType

class NXOpen.ShapeSearch.ShapeSearchBuilderOpenPartType

Bases: object

The open part type enum

Enum Members

Enum Member Enum Member Description
NotSetDisplayPart
Not set the opened part as display part
SetDisplayPartOnlyWhenOpen
Set the opened part as display part only when it doesn’t exist in the session
AlwaysSetDisplayPart
Always set the opened part as display part whether it exists in the session
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.