KinematicImportMcfBuilder Class¶
-
class
NXOpen.SIM.
KinematicImportMcfBuilder
¶ Bases:
NXOpen.Builder
Represents a builder for an import axis and channel data from mcf
Use the
Part
class to create a KinematicImportMcfBuilder object.New in version NX9.0.3.
Properties¶
Property | Description |
---|---|
IgnoreLimits | Returns or sets the flag which determines if the Limits of the MCF and the Kim are merge. |
McfPath | Returns or sets the path from the mcf file |
ReplaceChannel | Returns or sets the flag which determines if the channel data of the Machine Tool Builder are deleted befor they are replaced through the Channel data of the MCF-File |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
IgnoreLimits¶
-
KinematicImportMcfBuilder.
IgnoreLimits
¶ Returns or sets the flag which determines if the Limits of the MCF and the Kim are merge.
the soft limits are set based on the hard Limits of the Machine Tool Builder or if the limits in the mcf are useful they will be taken from MCF.
-------------------------------------
Getter Method
Signature
IgnoreLimits()
Returns: Return type: bool New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IgnoreLimits(replace)
Parameters: replace (bool) – New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
McfPath¶
-
KinematicImportMcfBuilder.
McfPath
¶ Returns or sets the path from the mcf file
-------------------------------------
Getter Method
Signature
McfPath()
Returns: The MCF Path Return type: str New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
McfPath(path)
Parameters: path (str) – The MCF Path New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
ReplaceChannel¶
-
KinematicImportMcfBuilder.
ReplaceChannel
¶ Returns or sets the flag which determines if the channel data of the Machine Tool Builder are deleted befor they are replaced through the Channel data of the MCF-File
-------------------------------------
Getter Method
Signature
ReplaceChannel()
Returns: Return type: bool New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReplaceChannel(replace)
Parameters: replace (bool) – New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
Method Detail¶
Validate¶
-
KinematicImportMcfBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.