KinematicAxisBuilder Class¶
-
class
NXOpen.SIM.
KinematicAxisBuilder
¶ Bases:
NXOpen.Builder
Represents the SimKimAxisBuilder class object
Use the
NXOpen.SIM.KinematicConfigurator
class to create a KinematicAxisBuilder object.New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
CoarsePrecision | Returns or sets the coarse precision. |
Direction | Returns or sets the axis direction |
FinePrecision | Returns or sets the fine precision. |
InitialValue | Returns or sets the initial value |
JerkLimit | Returns or sets the jerk limit. |
JumpVelocity | Returns or sets the jump velocity. |
Junction | Returns or sets the junction |
Kv | Returns or sets the kv. |
Limit | Returns or sets the axis limits flag |
LowerLimit | Returns or sets the lower limit |
LowerSoftLimit | Returns or sets the lower soft limit. |
MaxAcceleration | Returns or sets the max acceleration. |
MaxDeceleration | Returns or sets the max deceleration. |
MaximumVelocity | Returns or sets the maximum velocity |
Name | Returns or sets the kinematic axis’s name |
Number | Returns or sets the kinematic axis’s number. |
Tag | Returns the Tag for this object. |
Type | Returns or sets the axis motion |
UpperLimit | Returns or sets the upper limit |
UpperSoftLimit | Returns or sets the upper soft limit. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
KinematicAxisBuilderAxisDirectionType Enumeration | The axis direction type |
KinematicAxisBuilderAxisMotionType Enumeration | The axis motions type |
Property Detail¶
CoarsePrecision¶
-
KinematicAxisBuilder.
CoarsePrecision
¶ Returns or sets the coarse precision.
This defines the exact stop precision used to determine if a target point has been reached, so that the next NC-block can be executed.
-------------------------------------
Getter Method
Signature
CoarsePrecision()
Returns: the Coarse Precision Return type: float New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
CoarsePrecision(coarse)
Parameters: coarse (float) – the Coarse Precision New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
Direction¶
-
KinematicAxisBuilder.
Direction
¶ Returns or sets the axis direction
-------------------------------------
Getter Method
Signature
Direction()
Returns: the axis direction Return type: NXOpen.SIM.KinematicAxisBuilderAxisDirectionType
New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
Direction(axisDir)
Parameters: axisDir ( NXOpen.SIM.KinematicAxisBuilderAxisDirectionType
) – the axis directionNew in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
FinePrecision¶
-
KinematicAxisBuilder.
FinePrecision
¶ Returns or sets the fine precision.
This defines the exact stop precision used to determine if a target point has been reached, so that the next NC-block can be executed.
-------------------------------------
Getter Method
Signature
FinePrecision()
Returns: the Fine Precision Return type: float New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
FinePrecision(fine)
Parameters: fine (float) – the Fine Precision New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
InitialValue¶
-
KinematicAxisBuilder.
InitialValue
¶ Returns or sets the initial value
-------------------------------------
Getter Method
Signature
InitialValue()
Returns: the initial value Return type: float New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
InitialValue(initial)
Parameters: initial (float) – the initial value New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
JerkLimit¶
-
KinematicAxisBuilder.
JerkLimit
¶ Returns or sets the jerk limit.
The jerk limit value limits jumps in acceleration.
-------------------------------------
Getter Method
Signature
JerkLimit()
Returns: the jerk limit Return type: float New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
JerkLimit(jerk)
Parameters: jerk (float) – the jerk limit New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
JumpVelocity¶
-
KinematicAxisBuilder.
JumpVelocity
¶ Returns or sets the jump velocity.
The jump velocity define a lag time at the beginning of the motion.
-------------------------------------
Getter Method
Signature
JumpVelocity()
Returns: the jerk limit Return type: float New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
JumpVelocity(jump)
Parameters: jump (float) – the Jump Velocity New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
Junction¶
-
KinematicAxisBuilder.
Junction
¶ Returns or sets the junction
-------------------------------------
Getter Method
Signature
Junction()
Returns: the junction Return type: NXOpen.SIM.KinematicJunction
New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
Junction(jct)
Parameters: jct ( NXOpen.SIM.KinematicJunction
) – the junctionNew in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
Kv¶
-
KinematicAxisBuilder.
Kv
¶ Returns or sets the kv.
the Kv-Factor is a parameter of the drives. It influences the dragging error (difference between ideal motion profile and actual motion profile).
-------------------------------------
Getter Method
Signature
Kv()
Returns: the Kv Return type: float New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
Kv(kv)
Parameters: kv (float) – the Kv New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
Limit¶
-
KinematicAxisBuilder.
Limit
¶ Returns or sets the axis limits flag
This property is deprecated. Use
SIM.KinematicAxisBuilder.AxisMotionType`()
instead.-------------------------------------
Getter Method
Signature
Limit()
Returns: the axis limits flag Return type: bool New in version NX7.5.0.
Deprecated since version NX9.0.3: Use
SIM.KinematicAxisBuilder.AxisMotionType`()
instead.License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
Limit(onOff)
Parameters: onOff (bool) – the axis limits flag New in version NX7.5.0.
Deprecated since version NX9.0.3: Use
SIM.KinematicAxisBuilder.AxisMotionType`()
instead.License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
LowerLimit¶
-
KinematicAxisBuilder.
LowerLimit
¶ Returns or sets the lower limit
-------------------------------------
Getter Method
Signature
LowerLimit()
Returns: the lower limit Return type: float New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
LowerLimit(lower)
Parameters: lower (float) – the lower limit New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
LowerSoftLimit¶
-
KinematicAxisBuilder.
LowerSoftLimit
¶ Returns or sets the lower soft limit.
The soft limit on the real machine is checked by the controller to avoid that the machine travels into the mechanical stop (Hard Limit) with full speed (prevent damage)
-------------------------------------
Getter Method
Signature
LowerSoftLimit()
Returns: the lower soft limit Return type: float New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
LowerSoftLimit(lower)
Parameters: lower (float) – the lower soft limit New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
MaxAcceleration¶
-
KinematicAxisBuilder.
MaxAcceleration
¶ Returns or sets the max acceleration.
The maximum acceleration defines how fast the axis can accelerate.
-------------------------------------
Getter Method
Signature
MaxAcceleration()
Returns: the Max Acceleration Return type: float New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
MaxAcceleration(max)
Parameters: max (float) – the Max Acceleration New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
MaxDeceleration¶
-
KinematicAxisBuilder.
MaxDeceleration
¶ Returns or sets the max deceleration.
The maximum deceleration defines how fast the axis can decelerate.
-------------------------------------
Getter Method
Signature
MaxDeceleration()
Returns: the Max Deceleration Return type: float New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
MaxDeceleration(max)
Parameters: max (float) – the Max Deceleration New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
MaximumVelocity¶
-
KinematicAxisBuilder.
MaximumVelocity
¶ Returns or sets the maximum velocity
-------------------------------------
Getter Method
Signature
MaximumVelocity()
Returns: the maximum velocity Return type: float New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
MaximumVelocity(velocity)
Parameters: velocity (float) – the maximum velocity New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
Name¶
-
KinematicAxisBuilder.
Name
¶ Returns or sets the kinematic axis’s name
-------------------------------------
Getter Method
Signature
Name()
Returns: The axis’s name Return type: str New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – the axis’s new name New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
Number¶
-
KinematicAxisBuilder.
Number
¶ Returns or sets the kinematic axis’s number.
The axis number is used in cases where an axis is programmed through a number instead of through an address (e.g. on Siemens 840D: AX1=10 instead of X10).
-------------------------------------
Getter Method
Signature
Number()
Returns: The axis’s number Return type: int New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
Number(number)
Parameters: number (int) – the axis’s new number New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
Type¶
-
KinematicAxisBuilder.
Type
¶ Returns or sets the axis motion
-------------------------------------
Getter Method
Signature
Type()
Returns: the axis type Return type: NXOpen.SIM.KinematicAxisBuilderAxisMotionType
New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.SIM.KinematicAxisBuilderAxisMotionType
) – the axis typeNew in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
UpperLimit¶
-
KinematicAxisBuilder.
UpperLimit
¶ Returns or sets the upper limit
-------------------------------------
Getter Method
Signature
UpperLimit()
Returns: the upper limit Return type: float New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
UpperLimit(upper)
Parameters: upper (float) – the upper limit New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
UpperSoftLimit¶
-
KinematicAxisBuilder.
UpperSoftLimit
¶ Returns or sets the upper soft limit.
The soft limit on the real machine is checked by the controller to avoid that the machine travels into the mechanical stop (Hard Limit) with full speed (prevent damage)
-------------------------------------
Getter Method
Signature
UpperSoftLimit()
Returns: the upper soft limit Return type: float New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
UpperSoftLimit(upper)
Parameters: upper (float) – the upper soft limit New in version NX9.0.3.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
Method Detail¶
Validate¶
-
KinematicAxisBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.