ImportMachineKitBuilder Class¶
-
class
NXOpen.SIM.
ImportMachineKitBuilder
¶ Bases:
NXOpen.Builder
This class is used for the Import Machine Kit Dialog.
Calling
Builder.Commit()
on this builder will start the import machine kit process and return None.Use the
Part
class to import a Machine Kit object.New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
OutputDirectory | Returns or sets the machine kit output directory specify where the finished machine folder will be stored. |
PrintReport | Returns or sets the machine print report flat that specifies if a report will be plotted while import the machine or not. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
OutputDirectory¶
-
ImportMachineKitBuilder.
OutputDirectory
¶ Returns or sets the machine kit output directory specify where the finished machine folder will be stored.
-------------------------------------
Getter Method
Signature
OutputDirectory()
Returns: machine output directory Return type: str New in version NX11.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
OutputDirectory(outputDirectory)
Parameters: outputDirectory (str) – machine output directory New in version NX11.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
PrintReport¶
-
ImportMachineKitBuilder.
PrintReport
¶ Returns or sets the machine print report flat that specifies if a report will be plotted while import the machine or not.
-------------------------------------
Getter Method
Signature
PrintReport()
Returns: print report flag Return type: bool New in version NX11.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
PrintReport(onOff)
Parameters: onOff (bool) – print report flag New in version NX11.0.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
Method Detail¶
Validate¶
-
ImportMachineKitBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.