ReportManager Class¶
-
class
NXOpen.Report.
ReportManager
¶ Bases:
object
Represents the report manager.
To obtain an instance of this class use
NXOpen.Session.ReportManager()
.New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Preference | Returns the report preference. |
AutomationLogger |
|
CommandManager |
|
Methods¶
Method | Description |
---|---|
CreateResultXmlFileWriter | Creates a new NXOpen.Report.ResultXmlFileWriter object. |
GetOriginalImageDimension | Gets the original dimension of a given image file. |
Property Detail¶
Preference¶
-
ReportManager.
Preference
¶ Returns the report preference.
-------------------------------------
Getter Method
Signature
Preference()
Returns: Return type: NXOpen.Report.ReportPreference
New in version NX11.0.0.
License requirements: None.
AutomationLogger¶
-
ReportManager.
AutomationLogger
¶ Returns the
NXOpen.Report.AutomationLogger
belonging to the report managerSignature
AutomationLogger()
New in version NX11.0.0.
Returns: Return type: NXOpen.Report.AutomationLogger
CommandManager¶
-
ReportManager.
CommandManager
¶ Returns the
NXOpen.Report.CommandManager
belonging to the report managerSignature
CommandManager()
New in version NX11.0.0.
Returns: Return type: NXOpen.Report.CommandManager
Method Detail¶
CreateResultXmlFileWriter¶
-
ReportManager.
CreateResultXmlFileWriter
¶ Creates a new
NXOpen.Report.ResultXmlFileWriter
object.Signature
CreateResultXmlFileWriter()
Returns: Return type: NXOpen.Report.ResultXmlFileWriter
New in version NX11.0.0.
License requirements: None.
GetOriginalImageDimension¶
-
ReportManager.
GetOriginalImageDimension
¶ Gets the original dimension of a given image file.
Signature
GetOriginalImageDimension(imageFullFileName)
Parameters: imageFullFileName (str) – the full image file name Returns: a tuple Return type: A tuple consisting of (width, height). width is a float. height is a float. New in version NX11.0.0.
License requirements: None.