ProgramInformation Class¶
-
class
NXOpen.Report.
ProgramInformation
¶ Bases:
NXOpen.TaggedObject
,NXOpen.INXObject
Represents the program information for command automation.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
FunctionName | Returns or sets the program entry function name. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Language | Returns or sets the automation program language. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
ProgramFile | Returns or sets the automation program executer file. |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
Prints a representation of this object to the system log file. | |
SetName | Sets the custom name of the object. |
Enumerations¶
ProgramInformationLanguageType Enumeration | Represents the automation program. |
Property Detail¶
FunctionName¶
-
ProgramInformation.
FunctionName
¶ Returns or sets the program entry function name.
CPlusplus language: the function name is the exported function following required interface, Java language: the function name is the exported java class name, CSharp, Vb and Python language: the function name is “Main”.
-------------------------------------
Getter Method
Signature
FunctionName()
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FunctionName(functionName)
Parameters: functionName (str) – New in version NX11.0.0.
License requirements: None.
IsOccurrence¶
-
ProgramInformation.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
ProgramInformation.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Language¶
-
ProgramInformation.
Language
¶ Returns or sets the automation program language.
-------------------------------------
Getter Method
Signature
Language()
Returns: Return type: NXOpen.Report.ProgramInformationLanguageType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Language(languageType)
Parameters: languageType ( NXOpen.Report.ProgramInformationLanguageType
) –New in version NX11.0.0.
License requirements: None.
Name¶
-
ProgramInformation.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
ProgramInformation.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
ProgramInformation.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
ProgramFile¶
-
ProgramInformation.
ProgramFile
¶ Returns or sets the automation program executer file.
CPlusplus language: the dll file, CSharp language: the CS file or CS dll file, Vb language: the VB file or VB dll file, Java language: the Jar file, Python language: the Py file.
-------------------------------------
Getter Method
Signature
ProgramFile()
Returns: the program file with full path Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProgramFile(programFile)
Parameters: programFile (str) – the program file with full path New in version NX11.0.0.
License requirements: None.
Prototype¶
-
ProgramInformation.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
ProgramInformation.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
ProgramInformation.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
ProgramInformation.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.