CommandImporterOverrideOption Enumeration¶
NXOpen.Report.CommandImporter.OverrideOption is an alias for NXOpen.Report.CommandImporterOverrideOption
-
class
NXOpen.Report.
CommandImporterOverrideOption
¶ Bases:
object
Represents the override option when there is already a command existing.
Enum Members
Enum Member Enum Member Description Ignore No action, do not import to libraryReplace Import to replace the existing oneCopy Import and append a new one-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-