WorkPlaneGrid Enumeration

NXOpen.Preferences.WorkPlane.Grid is an alias for NXOpen.Preferences.WorkPlaneGrid

class NXOpen.Preferences.WorkPlaneGrid

Bases: object

Describes whether the Grid type selected is Polar or Rectangular

Enum Members

Enum Member Enum Member Description
Polar
Polar Grid
Rectangular
Rectangular Grid
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.