VisualizationHandlesHandleSizeValue Enumeration

NXOpen.Preferences.VisualizationHandles.HandleSizeValue is an alias for NXOpen.Preferences.VisualizationHandlesHandleSizeValue

class NXOpen.Preferences.VisualizationHandlesHandleSizeValue

Bases: object

Specifies size values for the default handle size.

Enum Members

Enum Member Enum Member Description
Small
Small Handle Size
Medium
Medium Handle Size
Large
Large Handle Size
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.