ViewVisualizationSpecialEffectsFogType Enumeration

NXOpen.Preferences.ViewVisualizationSpecialEffects.FogType is an alias for NXOpen.Preferences.ViewVisualizationSpecialEffectsFogType

class NXOpen.Preferences.ViewVisualizationSpecialEffectsFogType

Bases: object

Describes whether the fog type is selected as linear or light or heavy.

Enum Members

Enum Member Enum Member Description
Linear
Linear Fog
Light
Non linear Fog. Light fog produces a fog effect less pervasive than Heavy fog
Heavy
Non linear Fog
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.