SubdivisionModelingPreferencesDisplayModes Enumeration

NXOpen.Preferences.SubdivisionModelingPreferences.DisplayModes is an alias for NXOpen.Preferences.SubdivisionModelingPreferencesDisplayModes

class NXOpen.Preferences.SubdivisionModelingPreferencesDisplayModes

Bases: object

Display modes of subdivision cage and resulting body.

Enum Members

Enum Member Enum Member Description
CageAndBody
Display both cage and body
CageOnly
Display cage only
BodyOnly
Display body only
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.