SketchPreferencesDimensionLabelType Enumeration

NXOpen.Preferences.SketchPreferences.DimensionLabelType is an alias for NXOpen.Preferences.SketchPreferencesDimensionLabelType

class NXOpen.Preferences.SketchPreferencesDimensionLabelType

Bases: object

Describes the different options for displaying dimension labels.

Enum Members

Enum Member Enum Member Description
Expression
Displays the entire expression such as P2=P3*4
Name
Displays only the name of the expression, such as P2
Value
Displays the numerical value of the expression
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.