ShipbuildingLinesViewPreferencesShipbuildingLines Enumeration

NXOpen.Preferences.ShipbuildingLinesViewPreferences.ShipbuildingLines is an alias for NXOpen.Preferences.ShipbuildingLinesViewPreferencesShipbuildingLines

class NXOpen.Preferences.ShipbuildingLinesViewPreferencesShipbuildingLines

Bases: object

Geometry type

Enum Members

Enum Member Enum Member Description
Profile
Profile
Plate
Plate
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.