ShipDraftingViewLinesViewPreferences Class¶
-
class
NXOpen.Preferences.
ShipDraftingViewLinesViewPreferences
¶ Bases:
object
Represents set of Ship Drafting View Lines View Preferences applicable to drafting views.
Ship drafting view lines are used for the features in Ship Design To obtain an instance of this class use
Preferences.ViewPreferences.ShipDraftingViewLines()
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
GetColor | Get line color @return |
GetFont | Get line font @return |
GetShipDrawingObject | Get single line status @return status that determines SLR for the feature |
GetWidth | Get line width @return |
SetColor | The color of ship line. |
SetFont | The font type of ship line. |
SetShipDrawingObject | Note: The initial values are set based on the file NX_ShipAttribute. |
SetWidth | The width of hidden line or edges. |
Enumerations¶
ShipDraftingViewLinesViewPreferencesLines Enumeration | Line type |
Method Detail¶
GetColor¶
-
ShipDraftingViewLinesViewPreferences.
GetColor
¶ Get line color
Signature
GetColor(featureName, linesType)
Parameters: - featureName (str) – feature name e.g. decks, bulkheads etc.
- linesType (
NXOpen.Preferences.ShipDraftingViewLinesViewPreferencesLines
) – visible or hidden line type
Returns: Return type: int
New in version NX10.0.0.
License requirements: None.
GetFont¶
-
ShipDraftingViewLinesViewPreferences.
GetFont
¶ Get line font
Signature
GetFont(featureName, linesType)
Parameters: - featureName (str) – feature name e.g. decks, bulkheads etc.
- linesType (
NXOpen.Preferences.ShipDraftingViewLinesViewPreferencesLines
) – visible or hidden line type
Returns: Return type: New in version NX10.0.0.
License requirements: None.
GetShipDrawingObject¶
-
ShipDraftingViewLinesViewPreferences.
GetShipDrawingObject
¶ Get single line status
Signature
GetShipDrawingObject(featureName)
Parameters: featureName (str) – feature name e.g. decks, bulkheads etc. Returns: status that determines SLR for the feature Return type: bool New in version NX10.0.0.
License requirements: None.
GetWidth¶
-
ShipDraftingViewLinesViewPreferences.
GetWidth
¶ Get line width
Signature
GetWidth(featureName, linesType)
Parameters: - featureName (str) – feature name e.g. decks, bulkheads etc.
- linesType (
NXOpen.Preferences.ShipDraftingViewLinesViewPreferencesLines
) – visible or hidden line type
Returns: Return type: New in version NX10.0.0.
License requirements: None.
SetColor¶
-
ShipDraftingViewLinesViewPreferences.
SetColor
¶ The color of ship line.
The value should be between UF_OBJ_MIN_COLOR and UF_OBJ_MAX_COLOR.
Signature
SetColor(featureName, linesType, color)
Parameters: - featureName (str) – feature name e.g. decks, bulkheads etc.
- linesType (
NXOpen.Preferences.ShipDraftingViewLinesViewPreferencesLines
) – visible or hidden line type - color (int) – Color
New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SetFont¶
-
ShipDraftingViewLinesViewPreferences.
SetFont
¶ The font type of ship line.
Signature
SetFont(featureName, linesType, font)
Parameters: - featureName (str) – feature name e.g. decks, bulkheads etc.
- linesType (
NXOpen.Preferences.ShipDraftingViewLinesViewPreferencesLines
) – visible or hidden line type - font (
NXOpen.Preferences.Font
) – Font
New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SetShipDrawingObject¶
-
ShipDraftingViewLinesViewPreferences.
SetShipDrawingObject
¶ Note: The initial values are set based on the file NX_ShipAttribute.
xml The status determines the line settings for the ship feature in a view.
Signature
SetShipDrawingObject(featureName, singleLine)
Parameters: - featureName (str) – feature name e.g. decks, bulkheads etc.
- singleLine (bool) – status that determines SLR for the feature
New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SetWidth¶
-
ShipDraftingViewLinesViewPreferences.
SetWidth
¶ The width of hidden line or edges.
Signature
SetWidth(featureName, linesType, width)
Parameters: - featureName (str) – feature name e.g. decks, bulkheads etc.
- linesType (
NXOpen.Preferences.ShipDraftingViewLinesViewPreferencesLines
) – visible or hidden line type - width (
NXOpen.Preferences.Width
) – Width
New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)