SessionWorkPlaneObjectDisplay Enumeration¶
NXOpen.Preferences.SessionWorkPlane.ObjectDisplay is an alias for NXOpen.Preferences.SessionWorkPlaneObjectDisplay
-
class
NXOpen.Preferences.
SessionWorkPlaneObjectDisplay
¶ Bases:
object
Describes whether the object off work plane is normal display or dim and selectable or dim and non selectable
Deprecated since version NX8.5.0: See
NXOpen.Preferences.SessionVisualizationEmphasis
.Enum Members
Enum Member Enum Member Description Normal Normal DisplayDimAndSelectable Dim and SelectableDimAndNonSelectable Dim and Non Selectable-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-