SessionVisualizationScreenViewTriadLocation Enumeration¶
NXOpen.Preferences.SessionVisualizationScreen.ViewTriadLocation is an alias for NXOpen.Preferences.SessionVisualizationScreenViewTriadLocation
-
class
NXOpen.Preferences.
SessionVisualizationScreenViewTriadLocation
¶ Bases:
object
The view triad location types.
Enum Members
Enum Member Enum Member Description BottomLeft View triad display on the bottom left of the viewBottomRight View triad display on the bottom right of the view-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-