SessionVisualizationHighQualityImage Class

class NXOpen.Preferences.SessionVisualizationHighQualityImage

Bases: object

Represents the High Quality Image preferences for the entire session

To obtain an instance of this class, refer to NXOpen.Preferences.SessionPreferences

New in version NX4.0.0.

Properties

Property Description
Orientation Returns or sets the orientation for the High Quality Image (portrait or landscape).
PlotQuality Returns or sets the quality of the plot of the High Quality Image.
SubRegion Returns or sets the setting for whether the High Quality Image is generated from a sub-region.

Methods

Method Description
GetImageSize Returns the image size to use for the generation of the High Quality Image.
GetResolution Returns the resolution to use when generating a High Quality Image.
SetImageSize Specifies the image size to use for the generation of the High Quality Image.
SetResolution Specifies the resolution to use when generating a High Quality Image.

Enumerations

SessionVisualizationHighQualityImageImageSizeType Enumeration The size at which to generate a High Quality Image.
SessionVisualizationHighQualityImageOrientationType Enumeration Whether the High Quality Image is to be generated with portrait or landscape orientation
SessionVisualizationHighQualityImagePlotQualityType Enumeration Describes the quality desired when plotting the High Quality Image
SessionVisualizationHighQualityImageResolutionType Enumeration The resolution to use when generating a High Quality Image.

Property Detail

Orientation

SessionVisualizationHighQualityImage.Orientation

Returns or sets the orientation for the High Quality Image (portrait or landscape).

orientation is not used if image_size is fill_view or user_defined.

-------------------------------------

Getter Method

Signature Orientation()

Returns:
Return type:NXOpen.Preferences.SessionVisualizationHighQualityImageOrientationType

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Orientation(orientation)

Parameters:orientation (NXOpen.Preferences.SessionVisualizationHighQualityImageOrientationType) –

New in version NX4.0.0.

License requirements: None.

PlotQuality

SessionVisualizationHighQualityImage.PlotQuality

Returns or sets the quality of the plot of the High Quality Image.

plot_quality is not used if image_size is fill_view

-------------------------------------

Getter Method

Signature PlotQuality()

Returns:
Return type:NXOpen.Preferences.SessionVisualizationHighQualityImagePlotQualityType

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PlotQuality(plotQuality)

Parameters:plotQuality (NXOpen.Preferences.SessionVisualizationHighQualityImagePlotQualityType) –

New in version NX4.0.0.

License requirements: None.

SubRegion

SessionVisualizationHighQualityImage.SubRegion

Returns or sets the setting for whether the High Quality Image is generated from a sub-region.

sub_region is only used when image_size is fill_view

-------------------------------------

Getter Method

Signature SubRegion()

Returns:
Return type:bool

New in version NX4.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SubRegion(useSubRegion)

Parameters:useSubRegion (bool) –

New in version NX4.0.0.

License requirements: None.

Method Detail

GetImageSize

SessionVisualizationHighQualityImage.GetImageSize

Returns the image size to use for the generation of the High Quality Image.

x_size and y_size vary only for User Defined image size type. For other image size types, the values returned in them are the x and y sizes fixed for the image size type.

Signature GetImageSize()

Returns:a tuple
Return type:A tuple consisting of (imageSize, xSize, ySize). imageSize is a NXOpen.Preferences.SessionVisualizationHighQualityImageImageSizeType. xSize is a int. X Pixel size. See note above. ySize is a int. Y Pixel size. See note above

New in version NX4.0.0.

License requirements: None.

GetResolution

SessionVisualizationHighQualityImage.GetResolution

Returns the resolution to use when generating a High Quality Image.

The resolution is not used if the image_size is fill_view. dots_per_inch is variable only for User Defined resolution type. For other resolution types, the returned dots_per_inch is the number of dots per inch which is fixed for the given resolution type.

Signature GetResolution()

Returns:a tuple
Return type:A tuple consisting of (resolution, dotsPerInch). resolution is a NXOpen.Preferences.SessionVisualizationHighQualityImageResolutionType. dotsPerInch is a int. Dots per inch. See note above.

New in version NX4.0.0.

License requirements: None.

SetImageSize

SessionVisualizationHighQualityImage.SetImageSize

Specifies the image size to use for the generation of the High Quality Image.

x_size and y_size only apply for User Defined image size type. For other image size types, they are ignored.

Signature SetImageSize(imageSize, xSize, ySize)

Parameters:

New in version NX4.0.0.

License requirements: None.

SetResolution

SessionVisualizationHighQualityImage.SetResolution

Specifies the resolution to use when generating a High Quality Image.

The given resolution is not used if the image_size is fill_view. dots_per_inch is used only for User Defined resolution. For other resolutions types, the input dots_per_inch is ignored.

Signature SetResolution(resolution, dotsPerInch)

Parameters:

New in version NX4.0.0.

License requirements: None.