SessionUserInterfaceUIDisplayResourceBar Enumeration

NXOpen.Preferences.SessionUserInterfaceUI.DisplayResourceBar is an alias for NXOpen.Preferences.SessionUserInterfaceUIDisplayResourceBar

class NXOpen.Preferences.SessionUserInterfaceUIDisplayResourceBar

Bases: object

Describes whether the resource bar is displayed on left or right of window

Enum Members

Enum Member Enum Member Description
Left  
Right  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.