SessionSketchBackgroundType Enumeration

NXOpen.Preferences.SessionSketch.BackgroundType is an alias for NXOpen.Preferences.SessionSketchBackgroundType

class NXOpen.Preferences.SessionSketchBackgroundType

Bases: object

Describes the available sketch background types.

Enum Members

Enum Member Enum Member Description
Inherit
Sketch background color is inherited from the parent application
Plain
Sketch background color is forced to the plain background color
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.