SessionPmi Class¶
-
class
NXOpen.Preferences.
SessionPmi
¶ Bases:
object
Represents the set of PMI preferences applicable to entire session
To obtain an instance of this class, refer to
NXOpen.Preferences.SessionPreferences
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AssocHighlightColor | Returns or sets the associated highlight color |
ReadingDirection | Returns or sets the reading direction preference |
Methods¶
Method | Description |
---|---|
UpdateTrackingPropertiesFromXml | Update tracking properties |
Property Detail¶
AssocHighlightColor¶
-
SessionPmi.
AssocHighlightColor
¶ Returns or sets the associated highlight color
-------------------------------------
Getter Method
Signature
AssocHighlightColor()
Returns: Return type: int New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssocHighlightColor(assocHighlightColor)
Parameters: assocHighlightColor (int) – New in version NX4.0.0.
License requirements: None.
ReadingDirection¶
-
SessionPmi.
ReadingDirection
¶ Returns or sets the reading direction preference
-------------------------------------
Getter Method
Signature
ReadingDirection()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReadingDirection(readingDirection)
Parameters: readingDirection (bool) – New in version NX4.0.0.
License requirements: None.