SessionModelingSplineDefaultActionTypes Enumeration

NXOpen.Preferences.SessionModeling.SplineDefaultActionTypes is an alias for NXOpen.Preferences.SessionModelingSplineDefaultActionTypes

class NXOpen.Preferences.SessionModelingSplineDefaultActionTypes

Bases: object

Specifies the command that should be invoked when double-clicking on a spline.

The option applies to non-associative splines and Studio Spline features in the Shape Studio application only. .. versionadded:: NX7.0.0

Enum Members

Enum Member Enum Member Description
StudioSpline
Specifies Studio Spline for editing a spline
Xform
Specifies X-form for editing a spline
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.