SessionModelingSketchEditType Enumeration

NXOpen.Preferences.SessionModeling.SketchEditType is an alias for NXOpen.Preferences.SessionModelingSketchEditType

class NXOpen.Preferences.SessionModelingSketchEditType

Bases: object

Edit option for sketches

Enum Members

Enum Member Enum Member Description
InTaskEnvironment
Edit sketch in task environment
Direct
Edit sketch without entering task environment
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.