SessionModelingSketchDefaultActionType Enumeration¶
NXOpen.Preferences.SessionModeling.SketchDefaultActionType is an alias for NXOpen.Preferences.SessionModelingSketchDefaultActionType
-
class
NXOpen.Preferences.
SessionModelingSketchDefaultActionType
¶ Bases:
object
Double click action for sketches
Enum Members
Enum Member Enum Member Description EditWithRollback Edit sketch with rollback on double clickEdit Edit sketch without rollback on double click-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-