SessionModelingLinkedAndExtractedGeometryPropertiesInheritance Enumeration

NXOpen.Preferences.SessionModeling.LinkedAndExtractedGeometryPropertiesInheritance is an alias for NXOpen.Preferences.SessionModelingLinkedAndExtractedGeometryPropertiesInheritance

class NXOpen.Preferences.SessionModelingLinkedAndExtractedGeometryPropertiesInheritance

Bases: object

Describes whether the display of linked and extracted geometry properties inherits from parent object or part default

Enum Members

Enum Member Enum Member Description
ParentObject
Indicates that display of linked and extracted geometry properties inherits from parent object
PartDefault
Indicates that display of linked and extracted geometry properties inherits from part default
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.