SessionModelingDynamicUpdateType Enumeration¶
NXOpen.Preferences.SessionModeling.DynamicUpdateType is an alias for NXOpen.Preferences.SessionModelingDynamicUpdateType
-
class
NXOpen.Preferences.
SessionModelingDynamicUpdateType
¶ Bases:
object
Describes whether the Dynamic Update type is not selected or selected as incremental or continuous
Enum Members
Enum Member Enum Member Description NotSet Indicates that Dynamic Update type is not selectedIncremental Indicates that Dynamic Update type is incrementalContinuous Indicates that Dynamic Update type is continuous-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-