RoutingStockStockModeFlag Enumeration

NXOpen.Preferences.RoutingStock.StockModeFlag is an alias for NXOpen.Preferences.RoutingStockStockModeFlag

class NXOpen.Preferences.RoutingStockStockModeFlag

Bases: object

Describes the valid value for stock mode.

Enum Members

Enum Member Enum Member Description
LegacyStock
solid body in the work part, no component
StockAsComponent
component created with solid body in the component
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.