RoutingPathRadiusMethod Enumeration

NXOpen.Preferences.RoutingPath.RadiusMethod is an alias for NXOpen.Preferences.RoutingPathRadiusMethod

class NXOpen.Preferences.RoutingPathRadiusMethod

Bases: object

Describes method used to determine bend radius on a bend or sbend corner

Enum Members

Enum Member Enum Member Description
Radius
Use specified radius
Ratio
Use ratio to stock diameter to determine radius
Table
Use radius obtained from a bend table lookup
InnerRadius
Use inner radius
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.